What Is Off-Grid Manager?

Modified on Thu, 14 May at 6:03 PM


Off-Grid Manager Overview

Off-Grid Manager has two functions.

  • Keeping your home’s instantaneous power use (measured in watts) below a preset limit. This could be the maximum continuous output of a battery system or a generator.
  • When paired with compatible batteries, Off-Grid Manager disables devices (circuits) within the home as the battery's state of charge decreases, allowing the battery to energize the remaining loads for a longer duration.


Off-Grid Manager is only available when operating off-grid. Custom Controls and Panel Guard can be configured for on-grid load management.


Off-Grid Manager Power Management

When a grid outage occurs and Off-Grid Manager activates circuits will be managed according to their categorization:

  • Flexible Devices are powered by the batteries throughout the outage as long as the Power Limit is not exceeded.

  • Undesired Devices are immediately shed upon a grid outage and not re-enabled until five minutes after the return of the grid.


Flexible and Undesired Devices


How should I choose which circuits to classify as Flexible or Undesired and how should I prioritize them?


Flexible Devices are dynamic. The circuits at the top of the flexible list have higher priority than those below. A best practice is to place loads that will automatically resume, such as thermostatic loads (HVAC, water heater, etc.) or EVs, at the bottom of the list since they will be interrupted more often, and are good at recovering. On-demand circuits that do not operate automatically (dryer, oven, etc.) should be placed towards the top of the list, since interrupting these appliances often will reset whatever cycle they were attempting or have other side effects. When idle, these circuits will use minimal power and allow the lower-priority loads to cycle on and off. When active, the higher-priority loads will operate. If not enough power remains within the Power Limit, this will force the lower-priority Flexible Circuits to be temporarily disabled if necessary. Battery-integrated systems allow Flexible Circuits to be customized to shed at a specific battery state of charge percentage during a grid outage.


Undesired Devices are circuits you explicitly want to shed for the duration of the outage (unless overridden). Disabled circuits are not automatically resumed until five minutes after the grid outage is over. This is a good option for heavy loads that do not need to run during outages. Hot tubs and pool heaters are two examples. 


How long will Flexible Devices remain disabled?

Any disabled Flexible Circuit will remain so until there is enough available power to cover the predicted max power of that circuit. Note that there is a minimum disable time of five minutes to avoid rapid cycling of appliances.


How do I override control of a device/circuit?

Any disabled Flexible or Undesired Device can be manually re-enabled via the app by either the Home screen or Off-Grid Manager screen. However, if the Power Limit is exceeded again, the circuits will be re-disabled in ascending order. If you want one Flexible Device to take precedence over other Flexible Devices, you can reorder the device to be higher on the list.



Off-Grid Manager Power Limit and "Measured by" Devices


What is the Off-Grid Manager Power Limit? 

The Power Limit can be set by the installer or the owner of the system by selecting the pencil icon at the top of the Off-Grid Manager page, then select the "Maintain power limit of" card in the "I want to" section. Here you can enter the maximum allowable power consumption in watts (the Power Limit). If power on the "Measured by" Circuit(s) exceeds the Power Limit, Off-Grid Manager will disable Flexible Circuits in ascending order. Typically, the Power Limit should be set at or slightly less than the maximum continuous power output capacity of either the inverter or the battery, whichever is less (typically the battery-based inverter). Please note that in some systems, such as the Tesla Powerwall, the battery and the battery-based inverter are packaged together in a single enclosure that system owners likely think of simply as their “battery”. In these cases, there will be only one continuous power output rating provided by the manufacturer. 

In addition to continuous output capacity, all leading inverters also have a surge output capacity so that a total load greater than the continuous output capacity can be powered for a short time as motors and compressors start. To accommodate this, Off-Grid Manager will only start shedding controlled devices once a rolling three-second average of power on "Measured by" Circuit(s) exceeds the power limit. 


Off-Grid Manager Power Limit Example
 
By setting the Off-Grid Manager Power Limit to match inverter or battery maximum discharge limits, a larger number of circuits can be available off-grid without risk of tripping the inverter or damaging the battery. When the Power Limit is reached, Flexible Devices will be shed in ascending order (bottom of list to top) until power demand is once again safely below the limit. When power demand is safely below the Power Limits, Flexible Devices will be re-enabled in descending order (top to bottom) as long as each circuit’s predicted needs can be met by the available power supply. Five minutes after the grid is restored, Off-Grid Manager will return all circuits to their original pre-outage state. 


What are "Measured by" devices? 
"Measured by" devices are the circuits ReliaHome monitors and compares to the Power Limits. For most installations, the "Measured by" device(s) should be the circuit(s) that delivers battery power to the load center/electrical panel that ReliaHome controls. Off-Grid Manager will sum up measurements from any circuit(s) designated as a "Measured by" device and compare that instantaneous total power reading to the Power Limits. Note that in some cases where the "Measured by" device contains both PV and battery output, this limit will be extra conservative from a battery/inverter protection perspective, as some of the measured power could be coming from solar and not straining the battery inverter's output capacity.


Do I have to choose "Measured by" devices and Power Limits?
Yes. To ensure that your ReliaHome system functions well,  a Power Limit and at least one "Measured by" device must be selected during the setup process. This allows ReliaHome to manage the connected load and ensure it does not exceed the Power Limit.


Which circuits should I choose as "Measured by" devices?

Choosing the correct "Measured by" devices is crucial for proper operation. In general, only your CTs should be selected as "Measured by" circuits. If no auxiliary CTs are installed the main CTs will normally be selected. See the CT configurations below for more information. Only if no CTs are installed and all circuits in the load center are controlled by ReliaHome should you choose all controlled circuits as "Measured by" circuits.


Off-Grid Manager and CT Configuration


How should CTs be configured for proper Off-Grid Manager operation? 
ReliaHome Smart Panel CT configuration depends on the type of energy storage system and several other factors. The following are several basic configurations that will work properly with Off-Grid Manager:

  • Main CT-Only Configuration: Designate Main CTs as the "Measured by" devices(s) in Off-Grid Manager.
  • Main + Aux CT Configuration: Designate the Aux CT circuit as the "Measured by" devices(s) in Off-Grid Manager. (Note that this device may have been renamed to something like "Solar + Battery".)


If your installation does not resemble the drawings above, please see the following article for more information:


Further advice on proper CT placement and special configurations is available by contacting ReliaHome support at 888-421-0616 or support@reliahome.abb.com 


How does Off-Grid Manager work if there is more than one ReliaHome Smart Panel at my location?

Off-Grid Manager runs independently on each ReliaHome Smart Panel and can only interact with the devices (both Monitor and Control) measured by that ReliaHome Smart Panel. When more than one ReliaHome Smart Panel is installed at a location, all ReliaHome Smart Panels will be triggered by the same off-grid event detected by a single Grid Detection Circuit (GDC) branching off to each ReliaHome Smart Panel. Within the ReliaHome app, there will be one Off-Grid Manager per ReliaHome Smart Panel installed at the location, and each Off-Grid Manager instance will only control one ReliaHome Smart Panel.  


Note that each ReliaHome Smart Panel that runs Off-Grid Manager requires a dedicated "Measured by" device, or set of "Measured by" devices. This may mean that CTs from multiple ReliaHome Smart Panels are clamped on the same wires as shown in the example below. Note that there are many possible CT configurations and installers should carefully consider the configuration that best suits a particular site. Additional configuration information can be found here: CT Configuration Options


Off-Grid Manager Energy Management


Your smart panel's energy management feature prolongs the runtime of your home's battery in a grid outage by shedding Flexible Circuits as your battery discharges past the state-of-charge setpoint and re-enabling those circuits as the state of charge increases beyond the setpoint. 


This feature requires information about the battery's state of charge, which is accessed via an API request to the storage system. Not all battery manufacturers publish an API that is accessible to third-party platforms, so this feature is restricted to those systems that do. See the list below for storage brands that currently offer this feature:



A battery integration will need to be configured for your location before this functionality can be used. There are two ways to add a battery integration:

  • Option 1: Go to Settings > System > Devices & Integrations > Battery Integration
  • Option 2: Go to Controls > Off-Grid Manager > Add Battery

Select the battery brand and follow the on-screen prompts to integrate the battery state of charge with the ReliaHome Smart Panel. This process will normally require access to the battery or inverter monitoring account. 


For more information on battery integrations, see:


Customizing Battery State of Charge Settings


To edit the battery state of charge percentage at which an Flexible Circuit sheds:


1. Go to Controls > Off-Grid Manager.

2. Scroll to the bottom of the list of Flexible devices, select "Edit Battery State of Charge".
3. Adjust the slider to the desired percentage for each device.
NOTE: The maximum allowable percentage is 95%.













4. Select Done at the bottom of the screen.

The Flexible devices will update to the new percentages. They will shed at this percentage as the state of charge decreases, and it will be re-enabled when the state of charge reaches 5% greater than the shed threshold.



If you have additional questions about Off-Grid Manager, please contact 888-421-0616 or support@reliahome.abb.com 

Was this article helpful?

That’s Great!

Thank you for your feedback

Sorry! We couldn't be helpful

Thank you for your feedback

Let us know how can we improve this article!

Select at least one of the reasons
CAPTCHA verification is required.

Feedback sent

We appreciate your effort and will try to fix the article