Integrating Battery State of Charge with Off-Grid Manager

Modified on Mon, 6 Oct, 2025 at 5:01 PM

Manufacturer-specific battery integrations allow the ReliaHome Smart Panel to manage devices according to the battery's state of charge. As the battery discharges below a preset charge percentage the ReliaHome Smart Panel will shed Flexible Devices to increase battery runtime. As the battery recharges above the preset state-of-charge threshold the ReliaHome Smart Panel will re-enable Flexible Devices.


*Note that 50% state of charge is the default threshold at which Flexible Devices shed. You can edit each Flexible Device to shed at your desired percentages on the ReliaHome Smart Panel app's Off-Grid Manager screen. For more information on battery state of charge settings, see:


Battery State of Charge Integration Instructions:


Tesla Powerwall (Cloud)

Tesla Powerwall State-of-Charge-Based Control:

Smart panel users wishing to add Powerwall integration must obtain the Tesla Site ID following the process outlined below. Note that this process can only be performed on the mobile app. Do not attempt this using a browser via the reliahome.abb.com webpage interface.


In the ReliaHome Smart Panel app:

1. Navigate to the Battery Integration page via either option:
  • Option 1: On the Devices or Controls tab, select the "+" icon > Manage Devices & Integrations > Battery Integration.
  • Option 2: Select Controls > Off-Grid Manager > Add a battery to your system.
2. Choose Tesla (Cloud).
3. Choose Okay when prompted with a redirect notice to Tesla Powerwall.

Ensure the email address you use to log in to Tesla is the primary email address associated with your Powerwall. If the battery is not displayed on your Tesla app home screen, you are not logged into the primary account. See Tesla Powerwall State of Charge Integration Troubleshooting for more information.
4. Enter the primary email associated with your Tesla Powerwall account. This is normally the homeowner account. Select Next.
5. Enter the password for your Tesla Powerwall account and select Sign In.
7. After the Tesla sign-in process is complete, the app should redirect you to a Connection Status page.

Select "Test Connection".
8. Wait while the connection is tested.
9. Select Prioritize Devices once connected.
The Off-Grid Manager screen will display the Powerwall's state of charge. If desired, you can categorize your circuits and set the percentage you want your Flexible Devices to shed at when grid power is unavailable. For more information, see:



Tesla Powerwall State of Charge Integration Troubleshooting

The Site ID will not populate in Step 10 if a non-primary Tesla account was used to fetch the Site ID. If you encounter this issue:


Determine the Primary Email for a Tesla Account

To check which account is the primary email in Tesla:

1. Log in to the Tesla app.
2. Check if the Powerwall battery is displayed on the Tesla app's home screen.
  • If it is, select the three bars in the top right corner of this screen.
  • If it is not, log out and repeat Step 1 with the login credentials of another associated Tesla user (for example, a partner or family member).
The Tesla app’s home screen.
3. Select the name and email listed on the Tesla app's Menu screen.
The Menu screen of the Tesla app. The account holder’s name and email are at the top of the screen next to a user image.
4. Choose Personal Information.
The account profile page of the Tesla app. Personal Information is the first option listed.
5. Confirm the email address listed under Primary Email.
The Personal Information screen of the Tesla app. Primary Email is second in the list.


Follow the Powerwall integration instructions and use the primary email for Step 5 after you've redirected from the ReliaHome app to Tesla.



Remove Access from a Non-Primary Email Tesla Account

To remove access:

  1. Look for an email sent from Tesla confirming the addition of ReliaHome to the account and click the remove access link.
  2. Sign in to the Tesla page using the same incorrect (non-primary) login credentials.
  3. Uncheck the box granting permission and click Remove Access.
  4. Select Yes on the second page that appears and asks if you are sure to unlink the accounts.


Follow the Powerwall integration instructions again and ensure that you use the correct Tesla account with the primary email address.


Enphase

...

EG4

EG4 battery integration allows the ReliaHome Smart Panel to manage circuits according to the battery’s state of charge. As the battery discharges, the ReliaHome Smart Panel will disable Optional Circuits to increase battery runtime. As the battery recharges, the ReliaHome Smart Panel will re-enable Optional Circuits. 

 

Note: The default threshold for disabling/enabling a circuit is 50% state of charge. You can customize each Optional Circuit to shed/reenable at whatever percentage you desire via the ReliaHome Smart Panel app. For more information, see: What is Smart Power Mode? 

 

ReliaHome requires EG4 API access in order to receive state-of-charge information from the EG4 platform. The only information necessary to create API access between the two platforms is the EG4 inverter serial number. There are three ways to obtain the inverter serial number:


Method 1: Use the EG4 web platform: 1. Login to the EG4 Monitor Center user                  account: 

2. If you are a user of multiple stations, select the corresponding station (EG4 installation) using the leftmost dropdown menu. 

3. Make note of the inverter's serial number in the rightmost dropdown menu.  


Method 2: Using the EG4 Monitor App on a Mobile Device1. Login to the user account on the mobile app.

2.  If you are a user of multiple stations, select the corresponding station (EG4 installation) using the leftmost dropdown menu.

3. Locate the serial number on the right-hand side of the menu.
Method 3: Gathering information from the side of the inverter
The serial number can be taken directly from the inverter. Location of the S/N will differ depending on inverter model.
EG4® 6000XP Off-Grid Inverter
See the left-hand side of the unit to locate the serial number. 
EG4® 12kPV Hybrid Inverter
See the right-hand side of the inverter to locate the serial number. 


EG4® 18kPV Hybrid Inverter
See the right-hand side of the unit to locate the serial number.


EG4 Integration ReliaHome Smart Panel app procedure

Once the serial number has been obtained, follow these steps in the ReliaHome Smart mobile app:

In the ReliaHome Smart Panel app:

1. Navigate to the Battery Integration page via either option:
  • Option 1: On the Devices or Controls tab, select the "+" icon > Manage Devices & Integrations > Battery Integration.
  • Option 2: Select Controls > Off-Grid Manager > Add a battery to your system.
2. Select EG4 (Cloud).
3. Enter the EG4 Site ID (Serial Number), and press "Test Connection".
4. Wait while the connection is tested.
5. Select Prioritize Devices once connected.
The Off-Grid Manager screen will display the EG4 system's state of charge. If desired, you can categorize your circuits and set the percentage you want your Flexible Devices to shed at when grid power is unavailable. For more information, see:

SolarEdge

Compatible Batteries

SolarEdge battery integration will work with the SolarEdge Home Battery and LG batteries paired with a SolarEdge inverter. Note that the ReliaHome API integration does not work with SolarEdge's StorEdge systems.

API Access with SolarEdge

ReliaHome requires SolarEdge API access to receive state-of-charge information from the SolarEdge platform. Within the SolarEdge mobile app or web platform, an installer should generate a site API key following the process outlined by SolarEdge.


Note: The following procedure is only available in Admin (installer) SolarEdge accounts. System owners (homeowners) should contact their installer for assistance with this process.


In the SolarEdge platform:

1. Go to the Site Admin > Site Access > Access Control > API Access section.
The SolarEdge platform tab options. Included are: Dashboard, Layout, Analysis, Reports, Alerts and Admin.
2. Acknowledge reading and agreeing to the SolarEdge API Terms & Conditions.
3. Choose Generate API key.
4. Copy the key.
5. Select Save.
The API Access section of the SolarEdge platform.



In the ReliaHome Smart Panel app:

1. Navigate to the Battery Integration page via either option:
  • Option 1: On the Devices or Controls tab, select the "+" icon > Manage Devices & Integrations > Battery Integration.
  • Option 2: Select Controls > Off-Grid Manager > Add a battery to your system.
2. Select SolarEdge (Cloud).
3. Enter the SolarEdge Site ID / API Key, and press "Test Connection".
4. Wait while the connection is tested.
5. Select Prioritize Devices once connected.
The Off-Grid Manager screen will display the SolarEdge system's state of charge. If desired, you can categorize your circuits and set the percentage you want your Flexible Devices to shed at when grid power is unavailable. For more information, see:


API Security: The API Key provides access to information about your solar production, battery state of charge, and home energy consumption. Do not share the key publicly. Only share it privately with those with whom you wish to share this information. ReliaHome does not store API keys centrally and has no access to your private key, which is stored locally on the ReliaHome device.


For a full description of the SolarEdge API, please visit:





Was this article helpful?

That’s Great!

Thank you for your feedback

Sorry! We couldn't be helpful

Thank you for your feedback

Let us know how can we improve this article!

Select at least one of the reasons
CAPTCHA verification is required.

Feedback sent

We appreciate your effort and will try to fix the article

p { line-height: normal; /* Default spacing */ }