Stay Connected to your Smart Panel During an Internet Outage

Modified on Fri, 21 Nov, 2025 at 2:24 PM

Many modern smartphones include a system feature that automatically disconnects from a WiFi network when no internet connection is detected. While this behavior can be helpful in everyday use, it may prevent your device from staying connected to your home network during an Internet Service Provider (ISP) outage. The ReliaHome Smart Panel uses your home's WiFi network to communicate with your mobile device even when there is no internet connection, so it's important to understand how to maintain this connection when both grid power and internet are lost. 

Instead of allowing the automatic switching to cellular data that is often enabled by default on mobile devices, ReliaHome users can follow the steps below to ensure their devices still connect to the WiFi network. 


Note that when the internet is not available and these settings are implemented, you will only be able to communicate with your ReliaHome Smart Panel and will not be able to transmit or receive data from the internet. For this reason, we recommend only implementing these steps when you are experiencing an outage of both grid power and internet and we recommend that you revert to default WiFi settings when the internet outage is over, as the settings described below can negatively affect the usability of your device in typical environments where the WiFi signal may be weaker than a cellular signal.


During internet outages, only keep WiFi enabled when you need to communicate with your ReliaHome Smart Panel. Disable your device's WiFi connection when you need to navigate the internet. 



Follow the steps below for your device type:

iOS (iPhone / iPad)
WiFi Assist can cause the device to switch to cellular data when the WiFi connection is weak or offline. Turning it off helps ensure the device stays connected to your home network.


Disable Wi-Fi Assist:

  1. Open Settings
  2. Tap Cellular
  3. Scroll to the bottom
  4. Turn off Wi-Fi Assist

Optional: Improve WiFi Stability:

  1. Open Settings → Wi-Fi
  2. Tap the ⓘnext to your home network
  3. Make sure Auto-Join is enabled
  4. Ensure Private Wi-Fi Address is enabled (helps stability on some routers)

Android Devices
Many Android phones include features that automatically switch to mobile data or disconnect from Wi-Fi when the network has no internet. Disabling these features ensures your device stays connected during an outage.


Instructions vary by manufacturer. Use the steps below that match your device.


Google Pixel (Android 12–14):

  1. Open Settings
  2. Tap Network & Internet
  3. Tap Internet
  4. Tap the gear icon next to your WiFi network
  5. Tap Network settings
  6. Disable:
    • Switch to mobile data when Wi-Fi has no internet
    • Adaptive connectivity (optional)


Samsung Galaxy (One UI 4–6):

  1. Open Settings
  2. Tap Connections
  3. Tap Wi-Fi
  4. Tap the ⋮ menu in the top-right
  5. Select Intelligent Wi-Fi
  6. Turn off:
    • Switch to mobile data
    • Switch to better Wi-Fi networks (optional)
    • Turn on Wi-Fi automatically (optional)

OnePlus (OxygenOS 12–13):

  1. Open Settings
  2. Tap Wi-Fi & Network
  3. Tap Wi-Fi
  4. Tap your network’s gear icon
  5. Scroll to Wi-Fi Assistant
  6. Disable:
    • Smart Wi-Fi Switcher
    • Auto Switch to Mobile Data

 

Was this article helpful?

That’s Great!

Thank you for your feedback

Sorry! We couldn't be helpful

Thank you for your feedback

Let us know how can we improve this article!

Select at least one of the reasons
CAPTCHA verification is required.

Feedback sent

We appreciate your effort and will try to fix the article